WHEN.DRVHANDWHEEL

Description

Records the value of DRV.HANDWHEEL when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.

General Information

Type

R/O

Units

1/4,294,967,296 rev

Range

0 to 4,294,967,295 rev

Default Value

0 rev

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1170

No 32 bit No

M_01-05-11-000

Related Topics

DRV.HANDWHEEL | When